Hi ,
Please help to provide temp data for TPS3836K33DBVRG4.
Max Tj
θ JA
θ JC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user,
I am writing to update you on this thermal data.
Max Tj for this device is: 85 °C
RθJA is: 171.4 °C/W
RθJC(top) is: 105.2 °C/W
RθJB is: 42.1 °C/W
ΨJT is: 19.5 °C/W
ΨJB is: 41.8 °C/W
Thanks,
Abhinav.