This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Advanced BQMtester and EV2400

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50

I have an Advanced BQMtester board, HPA495 REV A and I have installed the Advanced BQMtester SW version 2.18.  SW installed correctly. All hooked up and connected to EV2400, I have powered the HPA495 REV A  board with 24V and 5V isolated power supply,  I have connected the BQ40Z50-R1 evaluation board as well with HPA495 Re B. When I try to run BQ tester station setup.exe   I get this error message.

Do I need to separately power the BQ40Z50-R1 evaluation board? 

Thanks and Regards

Dileep Chacko