Other Parts Discussed in Thread: BQ25713
IL_Avg function on bits 4..3 of the ChargeOption3 (34h) Register setting? It appears to be <10% of the 6, 10, or 15 amp settings and I would like to understand if this measurement senses and averages ACP/N 's differential voltage when Q1 is on to determine the average inductor current? Is this correct?
s the BQ25713 endowed with an micro inside or is it a pure hardware state machine?
We would also like to know if it supports I2C clock stretching?