Part Number: LMG1210
Other Parts Discussed in Thread: TIDA-01634
I'm intending to use the LMG1210 to drive a full bridge with EPC2020 FETs as shown in the image below.
The datasheet mentions the need for a 4 layer board. Is this necessary for low power applications or is it possible to get away with a 2 layer board? Maximum power over load will be 36W (12V into 4 ohm) switching at 500kHz.
Additionally, is there any issues with this circuit? particularly in terms of the bootstrap cap and diode?
Thanks.