Hi Team,
Input:12V Output:1V 15A(max)
The customer's issue is that output drops rapidly when the load is ON, resulting in the latter MCU rebooting. while if reduce the freq from 500kHz to 400kHz, the issue won't happen. So, what's the reason? customer can't reduce the freq and want to find the original reason to fix it.
according to the calculation, this design is in CCM, then how the freq affects the power level?
here is the SCH.
thanks!
Yang