I would like to know if it is possible to parallel two LM1084 to get 10A at 5V or would it better to use a pass transistor instead.
Thanks for the help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
It's possible to parallel two LDOs to get high current output with ballast resistors. You may find the following TI reference design helpful when you try to work on building a parallel LDO application. Using pass transistor is a different approach and it should work too.
There is another TI design that achieves 6A. Please see here:
http://www.ti.com/lit/ug/tidu421/tidu421.pdf
Regards,
Jason Song