Hi
Regarding 28722 the capacitor on VDD pin is mentioned is slau721a is 4.7 mfd, if I reduce to 2.2 mfd which parameter I should check so that functionality of UCC28722
should not get affected.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Regarding 28722 the capacitor on VDD pin is mentioned is slau721a is 4.7 mfd, if I reduce to 2.2 mfd which parameter I should check so that functionality of UCC28722
should not get affected.
Hi Rishabh,
I would suggest using equation 11 in section 3.3 in SLUA721A to calculate the minimum needed VDD capacitance. Too small of a capacitance could result in VDD falling to the VDD UVLO threshold during startup.
Best Regards,
Ben Lough