Hi team,
When I read the TLV758P datasheet, I didn't quite understand the Foldback Current Limit part. For example, let's say Vin=5V and Vout(NOM)=3V. Normal load=6ohm. So the foldback voltage is 0.4*3V=1.2V.
So if the load becomes to 3ohm, the Io should be 3V/3ohm=1A. But 1A is higher than the Icl so Io is restricted to Icl(take Icl=600mA). So the real Vout is 0.6A*3ohm=1.8V. Because 1.8V is higher than foldback voltage 1.2V, this conclusion works.
So if the load becomes to 1ohm, the Io should be 3V/1ohm=3A. But 3A is higher than the Icl so Io is restricted to Icl(take Icl=600mA). So the the real Vout is 0.6A*1ohm=0.6V. Because 0.6V is lower than the foldback voltage 1.2V, so the final Io is not 600mA. So my question is how to decide the final Io and Vout when the load is 1ohm? Thanks.
Best regards,
Wayne