I am designing an overvoltage crowbar circuit and I would like to use the TL431 as an adjustable comparator like in the circuit below (taken from Axotron's website): I will use a pot for R1 to adjust the "trigger" voltage.
I need to protect a 36V supply, so my circuit needs to trigger around 40V. Since the TL431 can output 36V max, I need to make some adjustments to the circuit. My first idea was adding a Zener diode in series with the TL431, connecting R2 to the anode of the TL431 (and cathode of zener) and anode of zener to ground. This makes the anode of the TL431 referenced to the zener voltage (for this example, let's use 10V). I will then set the TL431 to "trigger" at 30V. Will this cause any problems for the anode to be referenced to a voltage other than ground?