This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22958: Reverse Current blocking

Part Number: TPS22958
Other Parts Discussed in Thread: TPS22917, TPS22916, TPS2663

Hi <

Do TPS22958 block the reverse current from the O/P to I/P ?

Do you have a similar device which can switch Voltages from 4 V to say 40 V with a min 3 A Capability 

Regards

Eby Jayan

  • Hi Eby, 

    Thanks for reaching out on E2E!

    The TPS22958 does not have reverse current blocking, so any voltage that appears on the output pin will be reflected back onto the input through the body diode. If you're looking for a 5V load switch with reverse current blocking, I recommend looking at the TPS22916 or the TPS22917. 

    If you're looking for a higher voltage device, the TPS2663 might work here instead. 

    Thanks,

    Arthur Huang