Hi, Team.
May i ask you to know how much is the maximum output voltage of comp pin?
could you tell me how those pin works ?
it seems like that it is "output" pin type but there is not information about COMP pin.
could you tell me ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team.
May i ask you to know how much is the maximum output voltage of comp pin?
could you tell me how those pin works ?
it seems like that it is "output" pin type but there is not information about COMP pin.
could you tell me ?
Hi Masaharu,
The maximum voltage at comp pin is 6V.
Comp pin is the error amplifier compensation pin. Connect external compensation components to this pin to modify the error amplifier output. The error amplifier is internally current-limited so the user can command zero duty cycle by externally forcing COMP to GROUND.
You can refer to UCx84x datasheet there is detailed description for COMP pin.
Regards,
Teng
UC2845A datasheet doesnt show it .
Is it same meaning for UC2845A too?
even there is no description on UC2845A though.
Hi Masaharu,
It is same, The UCx84xA family of control devices is a pin-for-pin compatible improved version of the UCx84x family. They have same block diagram of FB and COMP pin part. In order to understand COMP pin better, it is necessary to understand the function block diagram and entire work process. And I suggest to refer to TI reference application.
Regards,
Teng