Other Parts Discussed in Thread: EV2400, BQEVSW, BQ27320, BQ27220
Hi,
Is it possible to run bq27200 drkr in EV2400?
And I'm looking for BQEVSW driver for bq27200.
Can anyone help me out.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
This is PCB Board is old model which has this BQ27200 and they were tested manually, I need to to auto testing.
That's the reason I'm asking. I need to find a way to make it work.
Hi Onyx,
I am working with Nhizanth on this:
We been able to communicate with the BQ27200 using Labview and EV2400. There's one issue we have is the conversion formula for Temperature measurements.
SLUS556D calls for this formula:
Temperature = 0.25 * (256 * TEMPH + TEMPL)
Temperature Registers (TEMPL/TEMPH) — Address 0x06/0x07
Here's what we read:
Read from 0x06: 0xA8
Read from 0x07: 0x04
We tried the formula from SLUS556D, it doesn't represent the expected temp.
Need your help on what should be the correct formula for Temp Measurement for BQ27200.
Hi Sime,
Did you figure this out yet?
For this case above, what is the actual temperature being measured.
Thanks
Onyx
Hi Corey,
Unfortunately we do not have sample code in labview to communicate with the device.
thanks
Onyx