Hi
My client is using BQ25606.
There are two questions regarding the Boost operation of the BQ25606.
1. If there is no adapter and the battery is present, does the battery operate when it falls below a certain voltage and is below the output voltage?
If so, is it possible to keep the output voltage constant?
2. If there is only battery and there is no battery, output voltage will be up down at regular intervals. Can this phenomenon be improved by adjusting the resistance of both ends of the TS pin? At present, the thermistor is not used, but the resistance of the lower end of the TS is increased.