Hi,
As per our requirement, we need 12 V@12 A output, and 12 V @22 A output from the 8 to 46 V. The Peak current up-to 96 V. So please guide us for selecting the correct part number.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Any Dual output BUCK boost channel converter Is available from TI?
Hi Vignesh,
Thanks for your question.
I do not think there are any dual output buck-boost channel converters available besides the TL1451, but I'm afraid that since the part is quite old, there are more recent parts that can fit your requirements better.
Please check the answer to this thread here:
https://e2e.ti.com/support/power-management/f/196/t/812214
In addition to this post, I would also recommend you to examine the LM5118, which is another buck-boost controller.
Thanks,
Richard
Hi sir,
But LM5118 up to 10 A only, Our requirement is 12 A. So i can't able to consider this IC.
instead of direct conversion any other alternate ways are available?
Hi Vignesh,
I'm currently thinking of a solution and will get back to you by the end of this week.
Thanks,
Richard
Hi Vignesh,
The LM5118 can handle more than 10A, but due to thermal constraints it is practical to limit it there.
I would suggest to take a look at PMP15035 as a starting point, which utilizes the LM5170 to generate a similar voltage rail as your requirements. The LM5170 also has multiphase operation capability which can be used to fit your current requirements.
You can also consider using the LM5175/LM5176 in a parallel configuration. You can see the references here:
http://www.ti.com/product/LM5176/technicaldocuments
Thanks,
Richard