Other Parts Discussed in Thread: TIDA-00318
Hi,
I would like to use a 20 mm diameter receiver coil with bq51003. The transmitter coil I use is WT202030-16M8-G (from TDK with 6.2 uH and 20 mm dia).
I looked at TIDA-00318 but could not find the coil used. Can you please send part number of the coil used in TIDA-00318? Also, what are the series and parallel capacitors to be used? Also, what is the max distance between receiver and transmitter coil I can expect the wireless charging to take place (when I use WT202030-16M8-G as transmitter coil and receiver coil used in TIDA-00318).
Thanks.