Hi:
I am triytng to use the lm3914 for a 3 series li-ion cell battery voltage indicator, in the range of 12.6 to 9 volts.
I found that i can stablish the low reference (pin 4)to 9 volts but the maximum range to the high reference (pin 6 nad 7) is 10.2 volts.
I don´t know if this is because of the 1.2 vd between pin 4 and 6 or is there any other way to have a high range (3 volts) to cover the full scale I am trying to use.
Thank
Carlos