Other Parts Discussed in Thread: GPCCEDV
Hi all,
I generated "GPCPackaged.zip" with bqstudio (based on 6 log files and 1 config file) and upload it to GPCCEDV. But the reply is "MiscInfo.txt" file containing the following message "ProcessType=CEDV".
The ProcessType was equal to 1. "ProcessType=1".
I un-zipped "GPCPackaged.zip" and changed this ligne in "config.txt" from "ProcessType=1" to "ProcessType=CEDV" and re-zipped "GPCPackaged.zip".
I then upload the new "GPCPackaged.zip" to GPCCEDV. But at this time, there is no reply from gpc_do_not_reply@ti.com.
What can be the problem ?