Other Parts Discussed in Thread: BQ76200
Hello, I am trying to make 2s Li-Ion Battery charger with cell Balancing. I am using charger IC BQ2057wsn and for cell balancing BQ29200. 3731.SCHEMATIC1 _ PAGE1.pdfCharger is working fine but cell Balancing is not working. battery charged with one cell 4.35V and other cell 4V.
Charger stops charging because one cell reached above threshold voltage(I am used here transistor to turn ON & OFF Charging using OUT pin of bq29200). Here is cell difference between two cell 0.35V.
so I want BQ29200 cell balancing should work here even after charging stop. but cell balancing is not working.
1)Please check schematic. I uploaded the schematic. is there anything wrong with schematic? BQ29200 is doesn't balance the cells.
2)Please verify Value of RCB1=RCB2=1KOhm, RVD= RCB=100 Ohm. CCD=0.33uf, CVD=0.1uf.
3) How much current consume BQ29200 to balance the cell & how much time required to balance the cell.