This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5160A: LM5160ADNT

Part Number: LM5160A

Tool/software: WEBENCH® Design Tools

Hello,

After I simulated the LT5160A with WEBENCH I used the WEBENCH design report as  a reference to make the circuit model with pSpice, the pSpice results are close to webench (thats great), but when I calculate the parameters from the data sheet I get different parameter, for example WEBENCH recommends L=82uH but from the data sheet equation I get Lmin=494uH.

How can I be sure that the circuit will work properly ?

Thanks in advance,

Rami S.