The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ12001: Can this device be paralleled?

Part Number: LMZ12001
Other Parts Discussed in Thread: LMZ36002, LMZM33602, LMZ23605

Hi,

Is it possible to parallel this device to provide up to 2A output current?

  • Hi Mosel,

    You can not parallel these two devices together because it does not have a ISHARE pin. Additionally, it does not have an external synchronization to synchronize the slave with the master.

    If you are interested in a 2A power module, there is a variety of different devices that may fit your needs. Below is a list:

    • LMZ36002 (QFN)
    • LMZM33602 (QFN)
    • LMZ23605 (Leaded)

    Regards,

    Jimmy