hi ,
Would you please help check if you can share the reference code of LM36011
Thanks a lot
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hope,
LM36011 enters stand-by mode from flash or torch mode and VLED Short Fault flag (bit [5]) of Flags Register
(0x05) is set, if the LED output experiences a short condition. An LED short condition occurs if the voltage at the
LED pin goes below 500 mV (typical). There is a deglitch time of 256 μs before the LED short flag is valid The
LED short fault can be reset to 0 by removing power to the LM36011, or setting the software reset field (Register
0x06 bit [7]) to a 1, or by reading back the Flags Register.
Since the device has a very low forward voltage, I suggest you can try connect a diode or a resistor serially with the 1MD03006, that may help to deal with problem. Please have try.
Regards
Sean