Hi team,
My customer would like to know the performance of load transient response of TPS62825 with following conditions. If you have a data with similar condition, could you share it?
1. Vin=4.5~5.5V, Vout=3.3V, Load transient range= 1A (e.g. 0.5A to 1.5A), Slew rate : 1A/us, target drop voltage = within 130mV.
2. Vin=4.5~5.5V, Vout=1.1V, Load transient range= 1A (e.g. 0.5A to 1.5A), Slew rate : 1A/us, target drop voltage = within 29mV.
Regards,
Yamaguchi