Hi everyone,
I'm using your product in order to switch the power for Asus Tinker board.
Without Asus board, it works properly. However, when connected Asus board, there are around 1.5V at the output although IC (EN pin is 0V) is disabled.
Also, the power led of the board is keeping ON and lots of peripherals of it runs.
I'd like the output voltage to be 0V when it's disabled.
(Note: There is a pull-down resistor is 100K at the output.)