Other Parts Discussed in Thread: GPCCEDV
Now , I want to use the GPCpackager to generate a package ,
but , I am not sure I used the rignt parameters :
Cell temination voltage in Volts : 3000(default) , I use 3500
Top SOC% interval to fit : 9 (default), I use 9 ,because I think it's OK
Bottom SOC% interval to fit : 3 (default) I use 9 ,because I think it's OK
I set Cell temination voltage in Volts to 3500, because I want the batttery not to discharge to a voltage under 3500.
What's the meaning of these parameters? and Have I set the right value?