This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD87330Q3D: Input voltage range

Part Number: CSD87330Q3D


Hello,

I'm designing a project that include CSD87330Q3D along with TPS65911A.

In the reference design, the input voltage for the CSD87330Q3D is 12V. in the typical application wrote Max. 12V Input.
I'll like to supply 5V to this pin. I'm not sure if it will work.

I'll appreciate any help and the calculations for the input voltage.

Regards,
Snir