Other Parts Discussed in Thread: BQ24105
Dear All,
**HIGH PRIORITY**
We are in need of a battery charging IC which will be the easiest to design. BQ24401 has a complicated design.
It must adhere to the following requirements:
1. The battery is of Ni-Mh.
2. The battery pack typical voltage is 3.6V(Max. 4.5V).
3. The input voltage is 5V.
4. Operating temperature: -40 to +85
Please provide an IC asap.
Regards,
Shruti