Hi,
I am interested if the above use case is safe for the TPS73733DCQR or if it can cause damage to it.
Device setup is as follows:
- Vin = 5V
- EN = Vin (5V)
- Vout (3.3V) may also be powered externally by a 3.3V.
Use Case:
- Power to Vin may abruptly be removed
- Vout still powered externally
My observation during this use case is that the Vout voltage is seen on Vin.
There is no way for me to disable EN before Vin is disconnected. So my observation seems to match the following from the datasheet "If the EN pin is not driven low, the pass element may be left on because of stored charge on the gate."
My question is if the above use case can cause damage to the TPS737.