Hi team,
The datasheet specifies that the maximum output voltage is 1.4V for TPS62362.
If the remote sense line has a parasitic series resistance, can the device output up to specified maximum voltage(1.4V)?
The reason why I ask is when the Vout equals the specified maximum voltage(1.4V) in the below configuration, the voltage at the right after the LC filter should be higher than the maximum voltage (>1.4V). Is it violate the datasheet specification of maximum output voltage?
Regards,
Saito