Hi Team,
My customer has a question regarding the GPOUT pin on the BQ27421-Q1.
In the datasheet it says that GPOUT should be pulled to VDD even if it is not used. Right now in their system they have this pin pulled high to the BQ27421-G1 1.8V rail and going to a GPIO on their host MCU. When the system is in shutdown (MCU off) the fuel-gauge stays ON and this 1.8V rail from the fuel-gauge remains high. Unfortunately this voltage leaks back into their system via the GPIO on the MCU. What happens if they do not keep GPOUT pulled high with the fuel gauge on? Will it cause unexpected chip behavior, or just increased current draw?
Thanks,
Mitchell