Other Parts Discussed in Thread: LMG1210
If I give -200V at input i.e. V(HS) will be -200 and PGND will be connected to GND.
In this case I will need to remove the bootstrap diode and give V(BST) from an external isolated supply
1)What should the value of V(BST) be?From datasheet 5V should be fine
2)Can V(BST) be continuous of should I control it externally so that it turns on when low side driver is on?
3)If I need to switch V(BST) externally can I use the LO output signal to control a FET?
4)What are the other ways of controlling V(BST)?