Hello,
I have a question about EMB1428Q. I have to use EMB1428Q independently.(Without EMB1499)
I give a pink signal (01010000) from MCU(SPO) to the EMB1428Q(SPI) and the EMB1428Q(SPO) give a yellow signal (1010 0101) back to my MCU(SPI) as shown in picture.
The blue line in the figure is the CLK.
But the outputs of the gate and resource have no reaction.
The way of the connection :
Fault 0,1, and 2 connect to ground
Connect EN with a NOT gate and give to DONE
Connect DIR with a NOT gate and give to DIR_RT
Question:
1.We are confused about the signal of the RST. Has anyone known the signal of the RST?
2.Does anyone meet the same situation or have any information about using EMB1428Q independently?
Thanks,
Zarkond