Other Parts Discussed in Thread: TPS92692
Hi team,
Could you support the following questions?
1. The d/s describes that " IADJ can be set to any value up to 2.54 V by connecting it to VREF through a resistor divider for static output current settings". Does this mean that the range of VADJ that can be analog dimming linearly is 0V to 2.54V?
2. According to the E.C table in the d/s, VADJ-MAX is specified as 2.46V(min), so should customer use VADJ is 0V to 2.46V?
3. If customer applies a voltage which out of the VADJ range to the IADJ-pin, how behave the TPS92641?
Regards,
Yamaguchi