Other Parts Discussed in Thread: LM5021
I'm using the LM5021 for the first time and I connected it as seen below. I not add the power plant yet, I just want to being the IC up. My thought were that once the IC was powered passed the UVL voltage that I should see at a minimum of 8V on the Vcc pin. Is this not the case? What is the minimum configuration to start up the chip?
KCJ