Part Number: TPS54618-Q1
for th TPS54618-Q1. How do I do remote sensing?
Will the following have instability problem?
On the same PCB, about 6”~8” max from the POL.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54618-Q1
for th TPS54618-Q1. How do I do remote sensing?
Will the following have instability problem?
Michael,
Generally I connect the top of the feedback divider after the last output capacitor. However, I have successfully connected it as far away as 6 inches. You do not need an additional 0 ohm resistor. Keep the resistor divider close to the IC. Make sure the FB trace is kept away from noise sources.