Other Parts Discussed in Thread: LM5170,
Hi I'Andy
Could LM5170 output 0V/25A??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm Andy
We want to use LM5170-Q1 in a new project.
There are 2 versions in this project.
Version1
The high voltage side is voltage range of 35V, the low voltage side is programmed power source 0V/20A-32V/6A.
Version2
The high voltage side is voltage range of 70V, the low voltage side is programmed power source 0V/10A-60V/3.5A.
I think the question is could LV works under 3V even 0V?
Hi Chun,
Thank you for reaching out. The short answer to you is yes the LM5170 can achieve this.
Note that the LM5170 can easily achieve a current source which is proportional to ISETA signal. It is just not very clear from you post:
The implementation will be different.
Thanks,
Youhao
Hi Youhao
Yes, it needs.
YES
Do you have any idea?
Thanks
Hi Youhao
The power can vary but you want the max power limit at voltage to not exceed 200W.
It is not a fixed watts power supply.
I think the question is could LV works/output 3V/20A even 0V/20A in Buck mode when HV is 60V?
The answer is YES. Like I mentioned, the LM5170 in the buck mode can implement the current source. See the EVM test results for output short circuit (Buck mode). The current after short is proportional to the ISETA signal. If you use single phase, set the ISETA=1V, and use 1mOhm resistor, you will limit the current to 20A no matter the output voltage.
If you use dual phase, reduce the ISETA by 2.
Thanks,
Youhao