This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5024: application question with I2C and flow chart

Part Number: LP5024


Hello expert,

Customer has below questions and could you kindly help to check on it? Thanks a lot!

Q1 : Do we have flow chart to initialize?

Q2 : About auto-increment function, could you give us example for it?

Q3 : Do we have I2C recovery architecture? Customer's EC team need recovery architecture to prevent I2C latch issue occurred.

Best regards,

Ann Lien

  • q1: You can refer to datasheet 8.4 Device Functional Modes.

    q2: It's simple. For example you want to write registers 00h to 09h, then you just need to send the address of 00h and then the 10 bytes data using auto increment.

    q3: LP5024 is i2c slave, so if the mcu send the correct i2c instruction then it responses.

  • Hello Kenneth,

    Thanks for reply. So for Q3, it means there is no I2C refresh architecture if we pull low I2C DATA/CLOCK to GND for certain period. Since they are afraid that I2C Bus is latch, they will recover I2C Bud through this architecture. Thanks a lot!

    Best regards,

    Ann Lien