Other Parts Discussed in Thread: LM5155
Hello I am trying to get output 24 2a by inputting Vin 6.2 ~ 7.4v using lm3481. Can I get output using lm3481?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for considering the LM3481 in your design.
I think given your power requirements, you can use the LM3481
Yes, there are some designs that can be used to output 24V @ 2A from your input ranges. I would recommend taking a look at PMP8536 and PMP8711 as a starting point, which use the LM3481 in a boost converter configuration.
There is also the LM5155, which is a newer version of the LM3481. Compared to the LM3481, it has lower quiescent current and higher efficiency. The LM5155BST-EVM also has your input range and can generate your output.
http://www.ti.com/tool/lm5155evm-bst
Thanks,
Richard