From TI BU comment that the bit[INIT] can’t be cleared by Host, but it is can clear this bit[INIT] easily by using TI tool. Please double confirm with BU does the way to clear bit [INIT] is reasonable or not?
As below is the test process and result.
We test that the bit[INIT] can be cleared by the way that send data 0x40 to command 0x01.
As below is the step:
1. Firstly, read Mode Register is 0x44, the bit[INIT] is enable;
2. Then write data 0x40, to command 0x01 (Mode Register);
3. Latest, read the command 0x01 (Mode Register), the read back value is 0x40, means the bit[INIT] is cleared.
The bit [INIT] is enable:
Write value 0x40 to command 0x01 to clear the bit [INIT]:
Scan the register again: