Hello, I am an Electrical Engineering student and would like some help with the following problem. I am using the LM1084 as an adjustable voltage regulator to output 5V at 5A as described in the datasheet. I printed a PCB to implement this design but it seems like the IC shuts off. I am using a 10uF Tantalum capacitor at the output as suggested and a 10 uF electrolytic capacitor at the input. I was also attempting to use a power transistor to output a higher current on a second design but since I cannot get the base design to function that design did not work as well and encountered the same problem. Is there something I am missing? I am using a 24V LiPo battery at the input and using a dummy load and cannot get more than 0.5 amps. I have done as much research into it as my knowledge allows me to so I was hoping someone can provide an idea as to why this is happening. Thank you very much.