Other Parts Discussed in Thread: UCC256404, UCC256302
Hi Sir,
I'm interested in a new device, the part number is UCC256404. YES, UCC256404, a new device. but, have a query.
our product is general inverter, system need a auxiliary power, we plan to use LLC controller UCC256404;
we don't need PFC stage, then the input of the device is 400Vdc from inverter power train Vbus,
The question is clear: Can HV PIN of UCC256404 connect to Vbus 400Vdc directly? Will this case affect the start-up of the LLC stage power?
Thanks and wait for your reply.
Regards.
-
Does it affect the power start