Other Parts Discussed in Thread: BQSTUDIO, EV2400,
It seems like no matter how I set the registers I am stuck at 10mA. I am using an EV2400 and BQStudio 1.3.86 with charger_1_00-bq25150.bqz as a configuration. Any suggestions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It seems like no matter how I set the registers I am stuck at 10mA. I am using an EV2400 and BQStudio 1.3.86 with charger_1_00-bq25150.bqz as a configuration. Any suggestions?
Hello Mike,
Can you please remove the J17 Vpullip jumper and check again to see if it works. Make sure Vio is shorted to VDD on J11
No luck, here is my register settings
* Created: Fri Jul 26 11:40:43 PDT 2019 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * Device: bq25150 * BQZ Container: Charger_1_00-bq25150.bqz * STAT0 01 STAT1 00 STAT2 00 FLAG0 00 FLAG1 00 FLAG2 00 FLAG3 00 MASK0 00 MASK1 00 MASK2 71 MASK3 00 VBAT_CTRL 4B ICHG_CTRL C8 PCHRGCTRL 82 TERMCTRL 14 BUVLO 00 CHARGERCTRL0 02 CHARGERCTRL1 42 ILIMCTRL 07 LDOCTRL B0 MRCTRL 2A ICCTRL0 10 ICCTRL1 00 ICCTRL2 00 ADCCTRL0 02 ADCCTRL1 40 ADCDATA_VBAT_M A894 ADCDATA_TS_M 55E0 ADCDATA_ICHG_M 002A ADCDATA_ADCIN_M 6B75 ADCDATA_VIN_M D961 ADCDATA_PMID_M D95C ADCDATA_IIN_M 03F8 ADCALARM_COMP1_M 2320 ADCALARM_COMP2_M 3890 ADCALARM_COMP3_M 0000 ADC_READ_EN 00 TS_FASTCHGCTRL 34 TS_COLD 7C TS_COOL 6D TS_WARM 38 TS_HOT 27 DEVICE_ID 20
Hello Mike,
Can you post your schematic?
Do you have /CE pulled low on your board?
yes I tried that, I didn't post the schematic because I was just using the EVM and you already have that. It's not an issue for me anymore because I am now using the GDK instead and it is working.