As shown in the figure above, I use DAC_FB_VEF1 to adjust output voltage of LM22676.
At most of the time, it works good. But when the ouput current is very low especially when it's lower than 30mA, the output volatge has a quite large ripple, which is about 2.5V, with a period 50~400ms(input voltage is 28V, output voltage is 22V). And it could hiccup repeatedly.
Could you help me with this problem?
Thank you.