Hi
My customer has question.Please cooperate me.
The specification of the customer is below.
Vin:12V
Vout:0.85V
IOUT:15~30A
→15A at the time of waveform measurement
fsw:300kHz
The waveform is disordered without the SW frequency performing constant operation.
Do you have any advice on the cause of this phenomenon?
There is also a circuit diagram etc. I can not place it here, so if you can tell me the e-mail address etc., I will send it locally.
Best Regard
T Kishi