This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: i2c

Part Number: BQ76920

Hello team, I'm currently working on a Mppt charger project and the BQ76920 is going to monitor and balance the battery pack. I need to provide the I2C communicaion with the microcontroller. In its datasheet, the maximum fall and rise time for SDA and SCL signals is provided as "0.40". I suppose its units are "microseconds", however I need to be sure about that. So my question is: What is the maximum allowed value for falling and rising time of I2C communication for BQ76920?

Thanks in advance.

Thanks