TPS5130: Is a soft start time of 170mS possible? The datasheet provides an equation to determine the capacitor value but no limit on how large it can be. Using that I get 460nF to produce 170mS, is that value of capacitance okay?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS5130: Is a soft start time of 170mS possible? The datasheet provides an equation to determine the capacitor value but no limit on how large it can be. Using that I get 460nF to produce 170mS, is that value of capacitance okay?
Hi Hogan,
It should be good.
Thanks!
Regards,
Hao