Other Parts Discussed in Thread: CSD17551Q3A
Hi TI Team,
I would like to confirm about FET selection for BQ25713 buck-boost circuit.
We need to change FET from AON7934 to FDMC007N30D .
The gate voltage rating decrease from 20V → 12V.
From the datasheet page 73, it says the gate drivers are internally integrated into the IC with 6 V of gate drive voltage.
So I assume there will be no problem. Can you kindly confirm?
Design parameters
Vin = 15V ~ 20V
Vout = 10V ~ 17V
Pout max = 45W
Best Regards
Naim