Other Parts Discussed in Thread: TPS2595
Hello team,
I want use TPS24751 on my hot swap product, I have some issues ,please help to confirm,due to the new product need to design, please help to review follow issues ASAP.
1. The input voltage is 3.3V, the input current is 0.3A, i want to control the inrush current, the inrush current is 0.3A, does TPS24751 meet the hot swap requirement?
2. On the datasheet, High ILimit Accuracy from 10 mA to 12 A, what's the lowest current can be Limited? 10mA or others? if the input voltage on the TPS24751 is 3V, the input current is 0.1A, does TPS24751 work normal?
Look forward to your reply, thanks.
kevin