This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561: SS/TR-to-reference crossover

Part Number: TPS54561


Hi, 

I have a design using TPS54561. I was trying to calculate the SS/TR capacitor value. From the description  7.3.8, it shows the internal reference is using 0.8V, I would assume the crossover point is when SS/TR voltage is above the internal reference 0.8V. However in electrical characteristics, it shows the crossover point if 1.16V. Could you please help explain the behavior of crossover? How could I use the 1.16V crossover point?

Thanks, 

Tony