Customer wants to convert single 12V input to multiple channels of 12V to different daughter cards. The power level is 40A input. Are there any suitable solutions for this requirement?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aki Li,
Please give us below information.
Hi Praveen,
Please check the latest requirement.
The input power level will up to 1200W.
3 output channels with 10A, 20A and 60A; OVP and OCP protection are needed.
Hi Aki Li,
We will have to realize this using a multi chip solution. Below are the IC's you can use for each rail,
There are many Hotswaps which can realize OVP and OCP. To start with you can have a look at TPS24720, TPS24770, LM25069. If telemetry is required, LM25066 is the best part.
For FET, we recommend using CSD16415
Let us know what you customer think of this solution.
Hi Aki Li,
Do you have any other questions ? If not, can we close this thread ?