Hi,
This is with reference and related to query raised with Thread Title "Need help to build DC power meter to measure energy up to 220V DC and 100A".
1. Is it possible to build the low voltage (Say 3.3V or 5V or 12V) from the incoming DC. We can not provide separate DC supply to rest of the circuitry.
Let me know how it can be possible and any design Idea.
This is with reference to design " http://www.ti.com/lit/ug/tidu849/tidu849.pdf " you have shared earlier with me in other thread title for DC power measurement up to 440V DC
2. How can we reduce the board size and power dissipation when we take input 220V DC for building low voltage supply on board for driving rest of the circuitry
Thanks